cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H723ZG Nucleo Board 144p, Super Low Power Consumption, Probably on Standby >10uA

Faizan_001
Associate II

Hello, 
I want to use the STM32 H723ZG Nucleo board 144p in my LoRaWAN project. For that, I need my microcontroller to consume less than 10uA of current in standby or sleep mode. Is that achievable? If yes, then,

1- What will be the hardware?

2- clock configurations?

3- What will be the configurations in the IOC file?

4- How can I not give power to the Ethernet port?

or if there is anything else i need to keep in mind.

0 REPLIES 0