cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H723ZG Ethernet

Srivatsan
Visitor

Hello everyone,

I am working with the NUCLEO-H723ZG board and attempting to establish Ethernet communication using TCP/IP. The firmware was built and flashed successfully using STM32CubeIDE version 1.19.0.

However, I am facing issues with basic network connectivity. Below are the details of my setup and observations:

Setup Details

  • Board: NUCLEO-H723ZG

  • IDE: STM32CubeIDE v1.19.0

  • Ethernet stack: LwIP

  • PHY interface: RMII

  • Flashing tool: ST-LINK (onboard)

  • Test performed: Ping test from PC

Observed Behavior

  • The Ethernet port LEDs (orange and green) remain solid ON after connecting the Ethernet cable.

  • Ping requests consistently fail (Request timed out).

  • No response is received from the board.

Troubleshooting Already Performed

  • Tested both Static IP and Dynamic IP (DHCP) configurations.

  • Verified IP address, subnet mask, and gateway settings.

  • Tried multiple Ethernet cables to rule out cable-related issues.

  • Rebuilt and reflashed the project multiple times.

  • Verified that the firmware flashes successfully and runs without build errors.

Despite these steps, the board does not respond to ping requests.

Questions / Assistance Required

  • Does solid ON state of both Ethernet LEDs indicate a known PHY or clock configuration issue?

  • Are there any known issues with RMII_REF_CLK configuration on the NUCLEO-H723ZG?

  • Are there specific CubeMX clock, MPU, or cache settings required for reliable Ethernet operation on STM32H723?

  • Any recommended minimal or verified example project for Ethernet ping testing on this board?

I need some guidance or suggestions to identify and resolve this issue.

Srivatsan_0-1768820714125.png

2 REPLIES 2
Srivatsan
Visitor

Here are some attachments, 

Hello @Srivatsan and welcome to the ST community;

This knowledge base may help you: How to create a project for STM32H7 with Ethernet and LwIP stack working

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.