cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 supports 802.1Qav?

graffiti
Associate III

Hi,

Checking the TRM for STM32H7 (RM0433) I see that in section 57.1 the following is listed as standards supported by the STM32H7:

  • 802.1-Qav-2009

However I see no references to tx queues or traffic shaping etc.

Does the STM32H7 support any 802.1-Qav-2009 features or is this a misprint in the TRM?

Thanks, Kieran.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Khouloud GARSI
ST Employee

Hi @graffiti​ ,

You are right. 802.1-Qav-2009 is not supported in STM32H7. This information will be removed from our reference manual.

Thanks for bringing this to our attention.

Khouloud.