cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 DMA

zhaowhong
Associate III

Hello
Can the STM32H743 modify data at two non-consecutive peripheral addresses in a single DMA event,A DMA event changes two peripheral addresses,

1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

There are 4 DMAs in 'H743, of 3 types.

The MDMA probably could do this on its own, through scatter-gather, but the MDMA can be triggered only by "high-profile" peripherals such as JPEG, QUADSPI, DMA2D, LTDC.

The remaining DMAs are triggered through their respective DMAMUX. Directly, neither of these DMAs can transfer to non-consecutive addresses; however, there may be a trick (costing one extra DMA stream): the DMAMUX, together with triggering its own DMA stream (transferring to the first address) can generate an Event upon every transfer (see DMAMUX_CxCR.EGE), that in turn can be set as trigger for the Request generator in the DMAMUX, and that can generate a trigger (request) for a different DMAMUX channel triggering a different DMA stream, transferring to the second address.

JW

View solution in original post

1 REPLY 1
waclawek.jan
Super User

There are 4 DMAs in 'H743, of 3 types.

The MDMA probably could do this on its own, through scatter-gather, but the MDMA can be triggered only by "high-profile" peripherals such as JPEG, QUADSPI, DMA2D, LTDC.

The remaining DMAs are triggered through their respective DMAMUX. Directly, neither of these DMAs can transfer to non-consecutive addresses; however, there may be a trick (costing one extra DMA stream): the DMAMUX, together with triggering its own DMA stream (transferring to the first address) can generate an Event upon every transfer (see DMAMUX_CxCR.EGE), that in turn can be set as trigger for the Request generator in the DMAMUX, and that can generate a trigger (request) for a different DMAMUX channel triggering a different DMA stream, transferring to the second address.

JW