cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 Performance at 1.8V

Fonzerelli
Visitor

Would STM32G4 performance gets effected if runs at lower voltage (1.8V)? Can the core clock run at max 170MHZ or it will run lower speed?

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

The max clock speed of some things will be lower at 1.8 V than at 3.3 V. For example, the max SPI speed is lower. You can see this in the datasheet.

TDK_0-1751492596464.png

 

 

However, the core clock can still run at 170 MHz at 1.8 V. No loss in performance there.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

The max clock speed of some things will be lower at 1.8 V than at 3.3 V. For example, the max SPI speed is lower. You can see this in the datasheet.

TDK_0-1751492596464.png

 

 

However, the core clock can still run at 170 MHz at 1.8 V. No loss in performance there.

If you feel a post has answered your question, please click "Accept as Solution".