cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0B1CET can't connect under SWD

jakobnator
Visitor

Hi,

I have built a handful  of STM32 designs before and never had a chip fail to connect. I can't seem to get any connection in Cube Programmer at all:

jakobnator_0-1741569762772.png

  • VDD,VREF+,VBAT is at 3.3V, VSS is connected to ground.
  • NRST is high at boot
  • I can see current drop from 17mA to 7mA (at 12V) when pulling NRST low , so it seems like MCU is doing something.
  • I originally connected with a JLINK but just bought a STLINKV3 SET with the same result.
  • Using SWD over a tag connect
  • tried every connect option in cube programmer (mode/reset mode)
  • I see SWCLK,SWDIO, and NRST working on an oscilloscope, although I haven't bothered decoding the signals.
  • I confirmed chip orientation
  • I confirmed SWCLK,SWDIO, and NRST pins
  • I confirmed my STLINK was updated
  • Checked for shorts under microscope

Schematic:

jakobnator_1-1741571188367.png

Layout:

jakobnator_2-1741571236810.png

 

I am pretty much out of ideas at this point, hoping its something *** I missed and need a second set of eyes :)

 

Any new ideas would be appreciated!

0 REPLIES 0