2017-08-28 8:03 AM
Hello,
I've been trying out the examples from the STM32 CubeF7 projects for the STM32F746G Discovery board, but when I build the LwIP application using the SW4STM32 tools the image is over 393MB and so too large for the target.
If build using Keil uVision the file size is tiny in comparison.
I'm able to build and deploy other apps such as the FatFS so confused as to why this should be?
2017-08-29 2:19 AM
I've done some more digging into this my examining the elf file that is also produced (attached).
Headers 4 to 6 are using the SRAM as a Physical location instead of a virtual one, therefore the bin file produced has to include the entire range from 0x08000000 (Start of FLASH) to 0x20000000 (start of memory) which explains the 393 MB bin file size as the file is mostly empty.
I think this will be initial variable settings, but headers 1 and 2 have similar but are correctly mapped from a virtual location in the FLASH to the physiical location in SRAM for initialisation.
Can anyone point me to whythese sections would be treated differently or where I should be looking next in my investigation?
________________ Attachments : STM32746G_DISCOVERY.elf.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyTN&d=%2Fa%2F0X0000000b8G%2FX5RSjF8OTHKV62CB3_Sm7hIceqoDyTxnJfnQuk_unmI&asPdf=false2017-08-29 4:26 AM
I see in the release notes that V1.2.0 has a change for this demo:
Use ETH buffers in SRAM instead of DTCM RAM for LwIP applications
and I see it is these buffers that are being 'incorrectly' mapped in the linkkerscript,ld file
Memory_B1(xrw) : ORIGIN = 0x20010000, LENGTH = 0x80
Memory_B2(xrw) : ORIGIN = 0x20010080, LENGTH = 0x80Memory_B3(xrw) : ORIGIN = 0x2004C000, LENGTH = 0x17d0 Memory_B4(xrw) : ORIGIN = 0x2004D7D0, LENGTH = 0x17d02017-08-29 4:44 AM
Solved it!
The NoLoad directives were missing at the end of the linkerscript file, they should read as follows:
.RxDecripSection (NOLOAD) : { *(.RxDescripSection) } >Memory_B1
.TxDescripSection (NOLOAD) : { *(.TxDescripSection) } >Memory_B2 .RxarraySection (NOLOAD) : { *(.RxBUF) } >Memory_B3 .TxarraySection (NOLOAD) : { *(.TxBUF) } >Memory_B4 ♯BIN file is now created with the correct size and can be downloaded and run.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.