cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 NAND FLASH ECC - Is Hardware BCH ECC Supported?

stcom9174
Associate II
Posted on September 06, 2016 at 11:59

Hello All,

If I am using one of the NAND FLASHes from Spansion (Cypress) such as the S34ML08G2 - is BCH ECC supported in hardware?

Thanks,

John W.

#stm43f7-fmc
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
Posted on September 06, 2016 at 15:21

RM0385 13.6.6:

The ECC algorithm implemented in the FMC can perform 1-bit error correction and 2-bit

 

error detection per 256, 512, 1 024, 2 048, 4 096 or 8 192 bytes read or written from/to the

 

NAND Flash memory. It is based on the Hamming coding algorithm and consists in

 

calculating the row and column parity.

 

 

JW

 

Posted on September 06, 2016 at 17:03

Generally there has been a movement to letting the NAND chips compute and check syndrome data as the bit level and array structures have become more exotic/complex. The chip vendor should be able to supply host level ''correction'' software/drivers that can resolve error flagged in the checking process.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
stcom9174
Associate II
Posted on September 08, 2016 at 12:24

Does ST have a list of compatible NAND FLASH memories for their microcontrollers?

Thanks.