2016-06-02 6:24 AM
Hi All,
The device is being used STM32F746BGTX.Set as follows. FMC_NORSRAM_TimingTypeDef Timing; /** Perform the SRAM1 memory initialization sequence */ hsram1.Instance = FMC_NORSRAM_DEVICE; hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE; /* hsram1.Init */ hsram1.Init.NSBank = FMC_NORSRAM_BANK1; hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE; hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM; hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_32; hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE; hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW; hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS; hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE; hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE; hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE; hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE; hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE; hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY; hsram1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE; hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE; /* Timing */ Timing.AddressSetupTime = 0; Timing.AddressHoldTime = 15; Timing.DataSetupTime = 1; Timing.BusTurnAroundDuration = 0; Timing.CLKDivision = 16; Timing.DataLatency = 17; Timing.AccessMode = FMC_ACCESS_MODE_A; /* ExtTiming */ HAL_SRAM_Init(&hsram1, &Timing, NULL);And when I tried to write multiple times to the same address to write NE1 does not work only once.ex)*(volatile uint32_t *)(0x60000000) = 0x11223344; <- pass*(volatile uint32_t *)(0x60000000) = 0x55667788; <- failWriting to the address other works properly.ex)*(volatile uint32_t *)(0x60000000) = 0x11223344; <- pass*(volatile uint32_t *)(0x60000004) = 0x55667788; <- passIs there a cache problem? Noncache to be the NE1 zone there any?I tried to change it as well as the optimization options.What's the problem?Thank you.
Best regards,gyosun.
2016-06-02 11:47 AM
The 0x60000000-starting area is cached, write back, by default. You could either disable the cache for that are in the MMU, or swap the FMC's ''NOR'' area for the area starting at 0xC0000000 using SYSCFG_MEMRMP.SWP_FMC. See AN4839, PM0253, and RM0385 of course.
JW2016-06-02 9:22 PM
Thank you for answer.
RM0385 Manual was set to see the MPU_RASR register as shown below.Thank you.
Best regards,gyosun.
2016-06-03 12:35 AM
Well, the answer is still ''I don't know'', but try also my other suggestion - the remap to 0xC0000000. The rationale behind this suggestion lies beyond the cache in the ''Device'' vs. ''Memory'' type of the two areas - the processor itself is allowed to merge accesses in ''Memory'' area.
JW2016-06-03 1:19 AM
gyosun, your problem is related to ARM architecture.
The region at 0x60000000 is defined as memory region, so it can use caches and (most important) write buffer. That last can merge and coalesce writes to the memory, this is exactly what happens to you. There are (at least) 2 solutions: 1) declare the region as Device or Strongly ordered, by reprogramming the MPU (don't trust your screen capture, MPU_RASR is a port, and currently related to a 128KB region starting at 0x20010000, according values in both MPU_RBAR and MPU_RASR). 2) use memory barriers instructions between your accesses (DMB/DSB, see the manual to understand difference between them). BTW, if there is memory behing 0x60000000, I will expect that merge or coalescing is not harmfull. What is the use case where writing twice the same memory area is absolutely required ?2016-06-09 5:22 AM
Thanks all,
When you write, as shown below and run the _DSB () function, even if the write to the same address works fine.But the gap between chip select is too large. read also the same.Is there any way to further reduce? Or Is it structurally impossible to?Thank you.
Best regards,gyosun.
2016-06-09 6:05 AM
Well, it's just the third time I write it: try the remap.
JW2016-06-09 6:47 PM
Write to the memory swap as follows seems well out the way you want.
But reading is still too big a chip select intervals.Is there any way to further reduce?Thank you.
Best regards,gyosun.
2016-06-09 11:53 PM
Your system clock appears to be the default 16MHz HSI, isn't it. Thus, there are about 9 cycles between the consecutive reads. That is about the maximum you can squeeze out from the processor.
Depending on your particular application, you might be better off using DMA. In that case you don't need to be concerned about cache and device/memory areas, as those relate only to the processor. If you want to get close to the possible extremums, you need to do a lot of manual reading and experimentation to get the knack. JW2016-06-13 5:41 AM
Thanks JW.
Spoken has been resolved by changing the HCLK clock to 216MHz, as the problem is completely.Thank you.
Best regards,gyosun.