cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery MEMS example won't output values

jim
Associate II
Posted on January 29, 2014 at 16:12

I'm running the MEMs example from

STM32F4-Discovery_FW_V1.1.0\Project\Peripheral_Examples\MEMS

using uVision / MDK-ARM and I'm not getting any changing values when the read function is being called on the SysTick interrupt. I am waving it around and tapping on it but not getting anything.

LIS302DL_Read(Buffer, LIS302DL_OUT_X_ADDR, 6);

printf(''values : %d %d\n'', Buffer[0], Buffer[2]);

values : 171 198

0xAB, 0xC6

These are the values that come through all the time. I've stepped into 

LIS302DL_Init

and 

LIS302DL_LowLevel_Init

but there's not conditional or information on how to see if it's failed. I have two of these board so I also tested on another board and it's the same. I think when I first got the board this was the application running on it so I don't think there is a hardware issue. 

Thanks,

Jim.

#stm32f4discovery-mems
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0