2013-07-21 9:42 AM
2013-07-22 1:19 PM
Not much into cameras and DCMI, but the screen shot seems to suggest you have the horizontal scan settings wrong, and not a multiple of the actual pixel count.
2013-07-30 11:53 PM
Thank you for the suggestion! I managed to get picture from the camera, the fault was in the python script, the picture resolution. But now I have another problem, the left side of the picture is black, but not solid black (maybe sensor problem?) and the resolution from the sensor seems to be not correct.
2013-07-31 8:31 AM
Look at horizontal blanking, and sync settings, or perhaps those for the front/back porch on the horizontal line signal.
2013-07-31 11:57 PM
I found out, that if I didn't change the resolution from the default 640*480 there is no black line, and the resolution is also ok. When I change the resolution to cif I receive 2 picture in 640 pixel width side-by-syde with black line. Maybe the camera did not crop the image, and sends windowed picture? The second attached picture's resolution is ok if I widen it to 2 picture.
I'll try to crop it with DCMI.2013-08-03 4:29 AM
The problem was with hstart hstop registers. I corrected them, and the image is fine now. Thank you for your help!
2013-08-14 1:53 AM
Can you send true form of code.
2013-08-15 5:53 AM
i will be happy if can you send your true code. thanks
2013-08-15 9:16 AM
What's the relationship between you two?
2013-08-16 5:43 AM