2012-10-02 1:50 AM
Hi!
I am trying to use the CS43L22 in a very simple way: only to amplify an analog signal created with the internal DACs of the STM32F4. On the Discovery board the output of DAC1 is routed to AINxx. So I create a 0-3V, 1000Hz saw tooth signal on PA4 (which I can measure). I also did the CS43L22 initialization via I2C and checked that all registers are set properly by rereading them and showing them on an attached LCD. I enabled the analog inputs, the mixers and the volume control. So that all is fine. In the CS43L22 data sheet I read about the init procedure and it says that I need a master clock on MCLK for the charge pumps of the internal amplifiers. So I use a timer to create a simple 7MHz rectangle singal for PC7 (which is routed to MCLK of the CS43L22). But: There is no output at all. I also tried to create beeps using the CS43L22 internal beep generator but I get nothing out :( I also have read the initialization procedures in the Audio Codec example carefully and used this for my code - but I am not able to get anything out of the earphone connector. When using the example alone, I can hear the repeating music file - so hardware should be ok. So my question is: is it ok to only clock MCLK for a working chip? Or is it mandatory to have a I2S signal? May I have overlooked something and I need more to get sound? Thank you for *any *hints, Chris2025-01-06 5:59 PM
Hi Kevin
Can get that example code which u checked for playing music