STM32F469xG STM32F469xE Flash memory organization
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-30 11:58 AM
Hi,
For the following devices:
STM32F469AE
STM32F469IE
STM32F469BE
STM32F469NE
Is the flash memory configured as single bank of 512KBytes? The RM0386 Reference manual does not not make it clear how the 512KByte flash is organized.
For the following devices:
STM32F469AG
STM32F469BG
STM32F469IG
STM32F469NG
STM32F479AG
STM32F479BG
STM32F479IG
STM32F479NG
Is the flash memory configurable to have dual bank? The RM0386 Reference manual does not not make it clear if only some STM32F4x9xG devices are dual bank configurable or all STM32F4x9xG devices are dual bank configurable.
Not all STM32F4xxxG devices are dual bank configurable. For instance, the STM32F417IG in only a single bank device, whereas the STM32F437IG is a dual bank configurable device. Both devices have 1MByte of flash.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-30 12:11 PM
Read RM flash section.
F40/ F41 single bank F42 F43 F46 F47 Dual bank- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-31 2:32 AM
Hi see.juan,
As mentioned in (3.3.1 Flash memory organization) part of the RM0386, the flash memory of all the 1Mb devicesSTM32F4x9xG
can be organized on dual bank by setting the DB1M option bit. Even DB1M is described as ''Dual bank 1Mbyte flash memory devices''. So, all 512 Kbytes devicesSTM32F4x9xE
, are with a single bank flash memory. -Hannibal-