cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446: Widen Access to High-Performance Line with Small Memory

Amel NASRI
ST Employee
Posted on December 11, 2014 at 16:04

0690X00000602w9QAA.jpg

STM32F446 product line enables high performance and rich connectivity into a highly integrated and energy efficient product, starting from 256K Flash.

The peripherals embedded in the STM32F446 include:

  • Up to 20 communication interfaces

  • 7x I2S audio interfaces

  • A SPDIF digital audio connection and a display parallel interface

  • A 90MHz Flexible Memory Controller (FMC) that simplifies control of external SRAM, SDRAM, Flash NOR/NAND, or LCDs with embedded controllers, and supports memory-remap mode for enhanced performance

  • A dual Quad-SPI (QSPI) interface that allows direct or memory-mapped connection to up to two external SPI NOR-Flash memories at single or dual data rate.

The STM32F446 is sampling now to lead customers. Volume production is scheduled for Q1 2015 in packages

from tiny

WLCSP81 (3.728mm x 3.85mm) to LQFP144 (20mm x 20mm) and with 256Kbyte or 512Kbyte Flash, all with 128Kbyte SRAM.

Budgetary pricing is from $3.75 for the STM32F446RC in 64-pin LQFP64 package with 256Kbyte Flash for orders of 10,000 pieces.

For further information please visit: 

http://www.st.com/stm32f446

.

#stm32f446

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0