cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F437-How to use 4KB backup SRAM as EEPROM?

Srujan G L
Associate II
Posted on November 16, 2017 at 09:17

Hi guys, 

            I'm using STM32F437IIH6 MCU, it has a 4KB backup SRAM which can be used as EEPROM like memory,

In order to achieve this we need to have a battery (3.3V coin battery) connected to the Vbat pin of the MCU.

I had worked on STM32F40-GEval board(STM32F407 MCU) and was successful in retaining the data in backup SRAM even after powering down the Eval board.

I designed a custom board with STM32F437 and inplemented the same(Battery connection to Vbat pin and all), but was unsuccessful in retaining the memory.

The data write was successful but the moment i switched off the MCU the data was gone.

where am i going wrong?

Thank You 

#stm32-sram #stm-32 #stm32f437 #stm3240g-eval #stm32f407 #stm32f437-backup-sram
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0