cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429i-Disco GPIO reset state

marabini
Associate
Posted on October 04, 2016 at 11:17

Hello,

I've a problem with the reset pushbutton state in the STM32F429i-DISCO: when I push the button I see that some pins are not in the three-state but are pulled down even if there are no other logic that make this work (pin PG5).

Another problem is that when I release the reset pushbutton, I see that the pins are pulled down until the FW takes the control. They are not in three-state status.

Thanks.

 
1 REPLY 1
Posted on October 04, 2016 at 18:13

PG5 connects to the SDRAM, what is that specified to do? The SDRAM also doesn't have an asynchronous reset connection.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..