cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 USB and FMC interoperability problem

zekeriya
Associate II
Posted on April 19, 2017 at 15:45

I am trying to use SDRAM (42S16400J) and NOR flash (M29W256GL) with STM32F429. With the code I generated with STM32CubeMX, Flash and SDRAM are working without problems. When I add USB-FS-OTG (device) to the project, the processor is blocked. The code is running when I turn off flash and SDRAM initialize operations. But with the first FMC operation I made while adding USB OTG to the project, the processor is blocked. I would like you to share if there is any reasoning about this problem.

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
zekeriya
Associate II
Posted on April 20, 2017 at 11:35

I changed the processor with Revision Y to revision 1.

I used USB_HS instead of USB_FS, but it did not change.

Using USB_HS according to the errata will prevent the error in other than Revision 3