STM32F429 SAI HAL_SAI_ErrorCallback errors OVRUDR
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-04-10 4:54 AM
Posted on April 10, 2015 at 13:54
Hi,
i'm using SAI output on STM32F429BIT6. I used some of the code from STM32CubeF4-Example stm324x9i_eval_audio.c for initialization. In pricipal all works fine, but sometimes i get an Error from the SAI interface and stop in the HAL_SAI_ErrorCallback() routine. Here is the content of the configuration and status-registers: SAI_ACR1: 0xc33280, SAI_ACR2: 0x1 SAI_ASR: 0x20001 SAI_ASR says it's an over or underrun error. Why does this happen? First i started playing audio with two small buffers in external RAM and sequentially fill them from an wav-file from SD-Card. Then i tried this with internal RAM, and also with an full RAM buffering, so there is no problem with SD-Card performance. Playing audio works for some files e.g. playing 5 files and then it stops. Sometimes it seems to look better when i set the DMA priority from DMA_PRIORITY_HIGH to DMA_PRIORITY_VERY_HIGH - but ths helps not at all. For Information: Audio stream is 8kHz, 16bit, Mono - so not much performance is needed. I also tried to record audio with SAI_Block_B into RAM and then play it by Block A from RAM. Recording works but when i start playing it sometimes calls the error handler. Dirk. #stm32f429-sai-dma-error-ovrudr
Labels:
- Labels:
-
SAI
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0