2016-09-21 6:30 AM
Hi,
I am using stm32f429ZIT6 mcu for my own board. I want to create 1 second interrupt with external 32.768Khz rtc but it doesn't work. My Systemclock config and rtc init functions are below:void SystemClock_Config(void){ RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct; __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 20; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 7; HAL_RCC_OscConfig(&RCC_OscInitStruct); RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5); PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC|RCC_PERIPHCLK_RTC; PeriphClkInitStruct.PLLSAI.PLLSAIN = 192; PeriphClkInitStruct.PLLSAI.PLLSAIR = 6; PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_4; PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE; HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct); HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}void MX_RTC_Init(void){ RTC_TimeTypeDef sTime; RTC_DateTypeDef sDate; RTC_AlarmTypeDef sAlarm; /**Initialize RTC and set the Time and Date */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc); sTime.Hours = 0x0; sTime.Minutes = 0x0; sTime.Seconds = 0x0; sTime.DayLightSaving = RTC_DAYLIGHTSAVING_SUB1H; sTime.StoreOperation = RTC_STOREOPERATION_RESET; HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD); sDate.WeekDay = RTC_WEEKDAY_TUESDAY; sDate.Month = RTC_MONTH_SEPTEMBER; sDate.Date = 0x19; sDate.Year = 0x16; HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD); /**Enable the Alarm A */ sAlarm.AlarmTime.Hours = 0x0; sAlarm.AlarmTime.Minutes = 0x0; sAlarm.AlarmTime.Seconds = 0x1; sAlarm.AlarmTime.SubSeconds = 0x0; sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_SUB1H; sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET; sAlarm.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY|RTC_ALARMMASK_HOURS|RTC_ALARMMASK_MINUTES; sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL; sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE; sAlarm.AlarmDateWeekDay = 0x1; sAlarm.Alarm = RTC_ALARM_A; HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD);}These codes are created by cubemx and i have created the callback function for rtc interrupt:void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc){ RTC_AlarmTypeDef sAlarm; HAL_RTC_GetAlarm(hrtc,&sAlarm,RTC_ALARM_A,FORMAT_BIN); //HAL_GPIO_TogglePin(GPIOG,GPIO_PIN_2); // HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_13); if(sAlarm.AlarmTime.Seconds>58) { sAlarm.AlarmTime.Seconds=0; } else { sAlarm.AlarmTime.Seconds=sAlarm.AlarmTime.Seconds+1; } while(HAL_RTC_SetAlarm_IT(hrtc, &sAlarm, FORMAT_BIN)!=HAL_OK){} }In callback function the pins must toggle every 1sn but it toggles at approximately 400ms.Any advise ??2016-09-21 11:40 AM
Hi rapid84,
I recommend that you check and run the RTC-Alarm example in the at this path:STM32Cube_FW_F4_V1.13.0\Projects\STM324x9I_EVAL\Examples\RTC\RTC_Alarm -Hannibal-2016-09-22 5:33 AM
Hi,
By the way i am using stemwin gui library for 320*240 tft LCD, when i use gui functions, the rtc collapses, and when i dont use gui functions rtc Works clearly. What may the reason be ?? Any advise..2016-09-22 8:04 AM
Hi rapid84,
What is the version of STemwin you are using ? and share the GUI configuration . -Hannibal-2016-09-22 9:32 AM
Hi,
I am using stemwin version 5.28 and if you ask the GUI_Config, it is like below:#define GUI_NUMBYTES (1024) * 150/*********************************************************************** Public code************************************************************************//*********************************************************************** GUI_X_Config** Purpose:* Called during the initialization process in order to set up the* available memory for the GUI.*/void GUI_X_Config(void) { // // 32 bit aligned memory area // static U32 aMemory[GUI_NUMBYTES / 4]; // // Assign memory to emWin // GUI_ALLOC_AssignMemory(aMemory, GUI_NUMBYTES); // // Set default font // GUI_SetDefaultFont(GUI_FONT_6X8);}I can not understand the relevance between the gui functions and rtc. Why does it affect the rtc working ?