2014-11-07 2:26 PM
Hi everyone.
I'm not sure what I did, but my F429 Discovery board is drawing way to much current. The overcurrent light (LD6) turns on when I supply the board with power and U8, which I believe is a power distribution switch, gets very hot. The board still functions, and I can still draw on the LCD with the simple paint program I was testing. Does anyone know if my board is toast or if I can replace some component/s to save it? A bit of background if it helps:Tried powering the board through a 5V regulator connected to an external power supply to the 5V pin. At this point, I noticed the current being drawn from my power supply seemed to be a lot (600mA). While trying to diagnose my circuit, I accidentally touched a wire from either the 5 or 3V pin to ground, and after that my board has been acting the way I just described. Any help would be appreciated.ThanksStone2014-11-13 6:38 PM
2017-12-07 12:53 AM
how did you replace it with the u8 on the board , I have a similar problem in my NUCLEO F767ZI board . Is it possible to replace the U4 on it.