cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 crashes after RCC configuration

kalhana
Associate II
Posted on January 25, 2016 at 19:50

Hi,

I have an issue with the STM32F429 (Discovery board with 8 MHz crystal).

I created a Keil project (software pack based) and added the following SW packs:

CMIS: Core

CMIS: DSP

Device: Startup

Then I added the following main file:

#include ''stdio.h''

#include ''stm32f4xx.h''

// PLL register values

#define PLL_MASK 0x80BC8000  // PLL register mask

#define PLLM_VAL 4           // PLL division factor

#define PLLN_VAL 180          // PLL multiplication factor

#define PLLP_VAL 0          // 0: div by 2

#define PLLSRC_VAL 1         // HSE is source to PLL

#define PLLQ_VAL 2           // PLLQ: not used

#define PLLR_VAL 2           // PLLR

int main(void){

  RCC->CFGR = (RCC->CFGR & 0xFFFFFF0F);           // AHB prescaler : 1

  RCC->CFGR = (RCC->CFGR & 0xFFFFE3FF) | 0x1400;  // APB1 prescaler: 4

  RCC->CFGR = (RCC->CFGR & 0xFFFF1FFF) | 0x8000;  // APB2 prescaler: 2

  

  RCC->CR |= 0x10000;

  while((RCC->CR & 0x20000) != 0x20000){  // wait for HSE ready

  }

  

  RCC->PLLCFGR = (RCC->PLLCFGR & PLL_MASK) | ((PLLR_VAL << 28) | (PLLQ_VAL << 24) | (PLLSRC_VAL << 22) | (PLLP_VAL << 16) | (PLLN_VAL << 6) | PLLM_VAL);  // Setup PLL

  RCC->CR |= 0x1000000;  // Main PLL: ON

  while((RCC->CR & 0x2000000) != 0x2000000){  // wait for PLL ready

  }

  

  RCC->CFGR = (RCC->CFGR & 0xFFFFFFFC) | 0x02;  // PLL_P is selected as system clock

  while((RCC->CFGR & 0x08) != 0x08){  // wait PLL_P to be used as system clock

  }

RCC->CR = RCC->CR & 0xFFFFFFFE;  // HSI oscillator disable

while(1){

}

}

But the CPU crashes after setting up the clocks. Any ideas?

Thank you.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on January 25, 2016 at 19:58

Flash wait states?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kalhana
Associate II
Posted on January 25, 2016 at 20:26

That was it. Thank you!

I spent hours trying to figure this out!