cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 controller is Reset when Power ON the Instrument

Sbira.2
Associate

I use STM32F429BIT6 controller in our instrument. When Power is ON after initialization STM32F429 controller is Reset. This happen only Once time after power on the instrument. It is not continuous reset.

What can i do

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

You're welcome!

When it works for you and your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

It it not necessary to use an external reset device due to the internal reset circuitry. Please try to remove:

  • R3, R6 (10k)
  • U3

After you've done this, only the reset buttons SW1 and C14 (100nF) are connected to NRST, which is fully sufficient.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you

You're welcome!

When it works for you and your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.