cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 Boot Slow

QingFeng
Associate II

Hello 

 I wrote a BootLoader program and an app program  in flash,BootLoader program will Jump to app. current state is,BootLoader boot takes a longtime,and jump also takes a longtime, the length of  time  positively correlated with the size of global variables in SDRAM,for example,if a 1M array defined in SDRAM,it takes about 1s,if a 15M defined used in SDRAM,it takes about 10s,i use the Keil IDE,and AC6 compiler. i think,the longtime is the BSS set to 0 takes,so i wrote the sct file like this  RW_SDRAM 0xC0000000 UNINIT 0X2000000
{
*(.SDRAM)
},the variables are defined like this uint16_t FrameBuffere[LCD_WIDTH*LCD_HEIGHT] __attribute__((section(".SDRAM"))); I want the variables in SDRAM not to be initialized,but it has no effect,Another article is very similar to my situation ,the solution is "Add the C compiler condition "--no_unaligned_access" to the APP",i I tried, it also has no effect,could you please help me,how to realize not init the SDRAM data.thanks a lot.

1 REPLY 1
TDK
Super User

Mark the SDRAM section as NOLOAD.

If you feel a post has answered your question, please click "Accept as Solution".