2016-06-30 1:25 PM
Hello, I have developed my code using IAR workbench, tried it on STM32F4 discovery board and it worked well. Now I want to download the code on STM32F407VGT6 chip I bought from digikey.com directly without the develop board, I connected it with hardware as described by st documentations and used SWD for programming and debugging but I always get an error message (No MC device found). Could someone help me to find what can cause this error?
Thanks in advance2016-06-30 2:12 PM
I've gone over this type of thing dozens of times on the forum, please review some of the other threads.
1-minute recap. Make sure the analogue supplies are connected. Review state on NRST pin. Make sure you have capacitors on the VCAP pins, and that you can see 1.25V on them. Check supplies. Check orientation. Check open/shorts. Provide a schematic, we have no idea what you've actually wired up.2016-06-30 3:08 PM
Here you are the schematic I used:
-I connect 6 capacitors 0.1uF in addition to 10uF between VDD and VSS and connected all VDD together and all VSS together, -I connected 2 capacitor 2.2uF ESR <2 Ohm between VCAP1, VCAP2 and VSS -I connected BOOT0 through 10KOhm resistor to VSS -I connected VDDA, VREF+ as shown in picture and VSSA to VSS -I connected NRST through 0.1uF to VSS -I used external crystal 8MHz with load capacitance 20pF and series resistance of 80Ohm, so I connected them to PH0, PH1 and used 400Ohm resistor -I connected st-link V2 programmer using SWD interface so I used PA14 as SWDCLK and PA13 as SWDIO but I put 2 resistors of 22Ohm between pins and programmer ________________ Attachments : schematics_001.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0jm&d=%2Fa%2F0X0000000bd5%2FBZaUQ6hgH710as6QVE9pYj.Shd4iK4eg8eXyW1dxnwE&asPdf=false2016-06-30 4:27 PM
The VCAP voltage test will tell you very quickly if the part is orientated correctly, and there is some potential the core will function/respond to SWD comms.
2016-06-30 5:34 PM
I tested the VCAP voltage but I got zero voltage so that means orientation may be wrong but if VDD and VSS were opposed that will damage the IC?
2016-06-30 6:53 PM
Verify the power pins and orientationHere are a couple of examples of pin/marking
https://community.st.com/0D50X00009Xka68SAB
Edit: Fixed DEAD LINK, original post from 30-Jun-2016
2016-08-06 5:06 PM
2016-08-06 8:43 PM
I would probably use the ST-LINK Utilities to do the testing here.
Is this the ST-LINK portion of the STM32F4-DISCO board? Have you disconnected the jumpers so it doesn't talk to the F4 part on the board? Your debug connectivity compose of NRST, SWDIO, SWCLK and GND?2016-08-07 8:05 AM
Yet I use the
ST-LINK
portion of the STM32F4-DISCO board, I had disconnected Jumper one(JP1) and connector three(CN3) to use this board as programmer. I use SWDCLK to PA14, SWDIO to PA13 plus 3.3V to VDD and GND to GND -first from discovery board and second to my circuit-. I tried to use this discovery as programmer to another discovery board with the same pins and it works, just removed JP1 from target board but I didn't use NRST pin while programming a discovery board with another one and every thing goes okay but I can't get the same result with my new circuit which is connect as recommended in hardware guide of ST.
2016-08-07 10:00 AM
Thanks a lot, When I connected the NRST pin with the ST-Link programmer, it works well.