cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f407VG using break input (ı could't understand it)

ataberktopcuuu
Associate II
Posted on June 07, 2016 at 14:55

Hi all, I try to understand break input.I read break input title in datasheet.Refer to  ''The break functionprotects power switches driven by PWM signals generated with the advanced timers.'' in  the datasheet. But I didn't understand power switches there.Which power switches? Can I only connect 3,3v or gnd to BKIN Pin(pA6).Can you give information briefly about it?Can you help me?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on June 07, 2016 at 15:02

Motor control type applications, using external power control circuits (switches) supplying higher current / voltages

Break Input, providing a means to leave the PWM outputs to the external switches in a safe state

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nesrine M_O
Lead II
Posted on June 07, 2016 at 15:09

Hi berk.ata,

I recommend you to have a look to the

http://www.st.com/content/ccc/resource/technical/document/application_note/1a/d5/a5/cd/98/4e/47/76/DM00080497.pdf/files/DM00080497.pdf/jcr:content/translations/en.DM00080497.pdf

 application note about STM32 device timer break feature 

-Syrine-

ataberktopcuuu
Associate II
Posted on June 07, 2016 at 15:38

I suppose ı understand.Briefly,Break input leave pwm outputs for  hold harmless motors etc(power circuit..) İs that so?

http://tureng.com/tr/turkce-ingilizce/so%20what%20you%27re%20saying%20is

 

http://tureng.com/tr/turkce-ingilizce/so%20what%20you%27re%20saying%20is