cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407VET

YZalo.1
Associate III

IMG_20241201_005100.jpgquestion.png

Sorry, can I use STM32F407VET and STM32F4 Discovery board in CUBE IDE version 1.17.0.
If so, tell me where I can find information on how to implement it.
I tried on STM32F404VET and when compiling, it says that it does not see the controller.Thank

1 ACCEPTED SOLUTION

Accepted Solutions

You have to use a st-link to connect to the f407 board. Do you??

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

6 REPLIES 6
YZalo.1
Associate III

sorry 

CUBE IDE version 1.16.0

STM32F407VET6

Should be able to build for the part# if you type it in properly

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
YZalo.1
Associate III

thanks, but what's the "part #", sorry

YZalo.1
Associate III

Sorry, and can I find a way to connect the above boards in some STM documentation.Thanks

You have to use a st-link to connect to the f407 board. Do you??

If you feel a post has answered your question, please click "Accept as Solution".
YZalo.1
Associate III

ok. i undertsend.generaly create .bin file in progect cubeide , and use him in st-link utility when conectet st-link v2 to board stm32f4 cross swdio and swclk pin's.

Thank