cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407G Discovery version D1 start-up failure using external power

rstanderregs
Associate
Posted on March 11, 2016 at 02:42

Hi All,

I have two STM32F407 discovery boards. A version B2 board and a new version D1 board.

The B1 starts on external power just fine with the same code but the D1 board does not. It only starts up after I connect it to a USB port while connected to the external power supply.

The external power comes from at computer power supply giving it 5.01V while the USB power comes from my Windows 7 Desktop. I think it gives it 4.97V.

Any idea what causes this weird start-up failure?

#stm32f407g-discovery
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on March 11, 2016 at 03:46

I'm pretty sure it isn't the difference in voltages.

If you are not using the USB/ST-LINK, disconnect it and the NRST from the target processor. I'm apt to think the issue is with the mbed firmware, rather than a board level issue.

I have no RevD boards, perhaps ST can send me some?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on March 11, 2016 at 10:16

You can buy some at the usual distributors, they appear to have plenty - it appears the old ones (with STLINK/V2) are already sold out and were restocked with these new ones (with the ''mbed-compatible'' STLINK/V2-1).

Unfortunately, ST chose to confuse us (and presumably themselves too) with a poorly chosen naming system.  The ''original'' F4 DISCO was labelled STM32F4DISCOVERY, the ''new one'' is STM32F407G-DISC1.

Also, the F4DISCO's materials (product page, UM) refers to STLINK/V2-A, which is presumably the same as STLINK/V2-1 mentioned elsewhere.

Another unfortunate fact is, that according to UM the serial inputs on STLINK/V2-1 are NOT connected to the target processor in any way (there are solder bridges on these lines on other STLINK/V2-1 - equipped DISCOs and NUCLEOs) and one is required to solder wires directly on the STLINK mcu's pins to use this - undoubtedly useful - facility.

It would be nice if somebody from ST could comment on all of above.

JW

rstanderregs
Associate
Posted on March 12, 2016 at 19:10

The problem was solved by upgrading the ST-Link Firmware from V2J25M14 to V2J26M15.

This same bug exists in V2J25M13 also.