2014-10-24 6:56 AM
I am trying to synchronise timer 3 and timer 4 to output a series of complimentary signals
I have timer 3 outputting a square wave at 1MHz and I want timer 4 to output a square wave at 5kHz (factor of 16). Timer 3 appears to be configured correctly and outputing the 1MHz signal however TIM4 is outputing a signal at ~30Mhz as just a short blip to logic 0. Not having chained timers before I am unsure of my configuration.#define GSCK_PWM_duty 50
#define GSCK_PWM_freq 1000000
#define GSCK_prescaler 0
#define timer3_freq 84000000 / (GSCK_prescaler + // 84,000,000
#define GSCK_PWM_count timer3_freq / GSCK_PWM_freq - 1 // 84 0x54
#define GSCK_PWM_duty_count ((GSCK_PWM_count +1) * GSCK_PWM_duty) / 100 - 1 // 41
#define XLAT_PWM_duty 50
#define XLAT_PWM_freq GSCK_PWM_freq/16 // 62500
#define XLAT_prescaler 0
#define timer4_freq GSCK_PWM_freq / (XLAT_prescaler + 1) // 1,000,000
#define XLAT_PWM_count timer4_freq / XLAT_PWM_freq - 1 // 16
#define XLAT_PWM_duty_count ((XLAT_PWM_count +1) * XLAT_PWM_duty) / 100 - 1 // 7
void tlc5941_init(){
tlc5941_IO_configuration();
GSCK_generator();
XLAT_generator();
}
void tlc5941_IO_configuration(){
GPIO_InitTypeDef GPIO_InitStruct;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
//Configure greyscale clocking pin for alternate function driven by timer
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStruct.GPIO_Pin = tlc5941_GSCK;
GPIO_Init(tlc5941_IOPORT, &GPIO_InitStruct);
GPIO_PinAFConfig(tlc5941_IOPORT, GPIO_PinSource6, GPIO_AF_TIM3);
GPIO_InitStruct.GPIO_Pin = tlc5941_XLAT;
GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_TIM4);
}
void GSCK_generator(){
TIM_TimeBaseInitTypeDef TIM_TimeBaseStruct;
TIM_OCInitTypeDef TIM_OCStruct;
//Clock config
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
TIM_TimeBaseStruct.TIM_Prescaler = GSCK_prescaler;
TIM_TimeBaseStruct.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStruct.TIM_Period = GSCK_PWM_count;
TIM_TimeBaseStruct.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStruct.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStruct);
TIM_Cmd(TIM3, ENABLE);
TIM_OCStruct.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCStruct.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStruct.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCStruct.TIM_Pulse = GSCK_PWM_duty_count;
TIM_OC1Init(TIM3, &TIM_OCStruct); //First comparator for Output
TIM_OC2Init(TIM3, &TIM_OCStruct); //Second comparator to drive XLAT
TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable);
TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable);
}
// XLAT latch pulse timing generator
// The XLAT pulse should be sent after the 16 pulse GSCK sequence has finished a cycle
// Therefore the timing factor for XLAT slaved to GSCK mush be factor of 16 it must also
// opperate at above 25hz to ensure addequate display refresh rates
void XLAT_generator(){
TIM_TimeBaseInitTypeDef TIM_TimeBaseStruct;
TIM_OCInitTypeDef TIM_OCStruct;
//Configure TIM3 CCR1 as internal trigger generator
TIM_SelectMasterSlaveMode(TIM3, TIM_MasterSlaveMode_Enable);
TIM_SelectOutputTrigger(TIM3, TIM_TRGOSource_OC2Ref);
//Set input signal for TIM4 as triggerx
TIM_SelectSlaveMode(TIM4, TIM_SlaveMode_External1);
TIM_SelectInputTrigger(TIM4, TIM_TS_ITR2);
//Start the peripheral clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
//Configure timer 4
TIM_TimeBaseStruct.TIM_Prescaler = XLAT_prescaler;
TIM_TimeBaseStruct.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStruct.TIM_Period = XLAT_PWM_count;
TIM_TimeBaseStruct.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStruct.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStruct);
TIM_Cmd(TIM4, ENABLE);
TIM_OCStruct.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCStruct.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStruct.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OCStruct.TIM_Pulse = XLAT_PWM_duty_count;
TIM_OC2Init(TIM4, &TIM_OCStruct);
TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable);
}
2014-10-26 3:07 AM