Skip to main content
ASSAAD.ASSAAD
Associate III
September 30, 2016
Question

STm32f407 problem in standby and wakeup

  • September 30, 2016
  • 5 replies
  • 1520 views
Posted on September 30, 2016 at 07:41

STm32f407 problem in standby and wakeup

    This topic has been closed for replies.

    5 replies

    ASSAAD.ASSAAD
    Associate III
    September 30, 2016
    Posted on September 30, 2016 at 08:13

    slimen
    Visitor II
    September 30, 2016
    Posted on September 30, 2016 at 11:23

    Hello,

    To more understand your issue, we need more details about your application and configuration.

    - Which Cube version using ?

    - Are you using CubeMX generated code ?

    - Did you added your own code or used one of the firmware examples from the STM32Cube packages?

    Regards

    ASSAAD.ASSAAD
    Associate III
    October 3, 2016
    Posted on October 03, 2016 at 10:49

    Hello ;

    Sorry I posted from mobile phone but it does not work .

    problem :

    we use standbye mode ; we noticed that while the MCU in the standby mode and the

    VDD is removed  then the VDD is reconnected ( this can happened while replacing the battery during standby mode) ; the MCU never wakeup it needs an hardware reset to start again; and since this is not possible in our product because Reset is inside the pcb ; can you suggest a solution for our problem ; please ?

    Thank you inadvanced

    Associate
    October 9, 2023

    Hi @ASSAAD.ASSAAD 

    we are also facing the same issue now did you got any solution please share here. It is very helpful for us.

    ASSAAD.ASSAAD
    Associate III
    October 4, 2016
    Posted on October 04, 2016 at 16:16

    Any suggestion here friends ?