cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 HS MSC read\write speed

boris239955_stm1
Associate II
Posted on August 08, 2012 at 15:37

HI,

I did connect STM32F407DESCOVERY to SMSC USB3320 ULPI (USB High Speed mass storage configuration). And uSD curd via SDIO interface.

The MCU configured to work in its maximum performance:

CPU clk 168Mhz , Enpoint 512byte + aditional endpoint enabled + USB DMA enabled

+ SDIO DMA Enabled.

However the maximum read\write speed for uSD cards of class 6 \class 10 is about

6 Mbyte\sec. When i connect these cards via card reader i get speeds of 20Mbyte at readings.

My quastion:

Is it maximum available speed (6MB\sec) that can be achieved using STM32F4 in MSC configuration ?

Do anybody  get better results ?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 08, 2012 at 23:12

No doubt because you have a number of serialized operations:

READ MULTIPLE SECTORS FROM SD CARD,

WAIT TILL COMPLETE,

SEND DATA OVER USB,

WAIT TILL COMPLETE,

REPEAT

In system where you get 15-20 MBps you've cut out several of these steps, and perhaps a bus or two.

Silicon implementation designed for MSC deliver the data directly from the mass storage device to the USB output stream with minimal latency/lag, and a hardware FIFO structure to provide some elasticity.

Of the ST examples I've observed you have TWO independent DMA operations, and minimal, if any, overlap between them.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
boris239955_stm1
Associate II
Posted on August 09, 2012 at 07:05

Thanks,

I see.

So to get maximum performance i need use some bridge usb-sd like

http://www.maxim-ic.com/datasheet/index.mvp/id/6226

To your openion the speed i get 6Mbyte\sec is somthing that

suites the STM32F4 limits or i can get more speed (up to 10 maby) ?

sameena shaikh
Associate II
Posted on October 23, 2017 at 11:10

Hi,

How did you measure the read write speed with which it is writing to or reading from sd card??

Thanks & Regards

Sameena Shaikh