Skip to main content
Visitor II
January 17, 2024
Question

Stm32f407 - Error "can't reset the core" with ST-Link.

  • January 17, 2024
  • 0 replies
  • 1108 views

Hello,

 

I am using STM32f407IGT6 with Keil uvision and HAL library. When I try to connect the device with ST-Link and flash the software using the JTAG interface, I always see "can't reset the core" as the error.

ajain20_0-1705490340060.png

BOOT0 - Connected to GND

BOOT1 - Connected to VCC

Can someone please help here?

This topic has been closed for replies.