stm32f407 encoder using MX bug ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-14 12:23 PM
Posted on December 14, 2015 at 21:23
i have used stm32f407 and timer 2 in encoder mode (in 4X mode) , but after long hours of debugging , i have found the problem with the IC1 and IC2 polarity , selecting this option will cause the timer to no count , while if Rising or falling edge is selected it works properly . why can this option be selected if it is not supported in this mode . and shouldnot it be used when working in TI12 mode ?
another thing is input filter calculation , datasheet is awful at showing how to calculate it and its relation with clock , instead F(dts) is used and N=x , with no figure for explanation
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0