STM32f407 and bootloader
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-03-05 2:52 AM
Posted on March 05, 2013 at 11:52
Hi
Is it possible to change the pins of the bootloader that is loaded inside the chip? As I read it is only usart3 and only on PORTB. Thank you
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-03-05 3:27 AM
Posted on March 05, 2013 at 12:27
Is it possible to change the pins of the bootloader that is loaded inside the chip? As I read it is only usart3 and only on PORTB.
Where are you reading this, and in what context? The pins are fixed, but you should be able to use USART1 (PA9/10), USART3 (PB10/11), USART3 (PC10/11) as well as CAN and USB options. The exact options will depend on the board design, the PA9 being a problem on the STM32F4-Discovery, but only because of the huge bulk capacitor attached to it by that design. See Table 22
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..