cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401VDT TO ESP12E WIFI MODULE THROUH SPI INTERFACE

amar2
Associate II
Posted on February 06, 2017 at 09:55

Hi Regnegade/everyone,

This is my skype user id:

mailto:amar.manda67@gmail.com

.

If you are free please ping to me because I need help for ESP12E wifi module

to interface with STM32F401VDT.

Why am sending skype ID,means it is easy to share things regarding ESP12E

module. 

Thank you sir.

2 REPLIES 2
Renaud BOUZEREAU
ST Employee
Posted on February 06, 2017 at 11:37

Hello, the STM32F769 discovery supports an Espressif wifi module: you can directly connect the Espressif module to the kit, with associated software available as an example in STM32Cube for STM32F769.

amar2
Associate II
Posted on February 07, 2017 at 08:09

Hi sir,

Thank you for reply me sir,

We are using ESP-12E in HSPI mode,but we are facing difficulty while communicating with ESP-12E in HSPI mode.

I have seen you supported for Arduino using SPI mode and we also want to implement similarly using STM32f4.

Link is given below for SPI support .

https://learn.sparkfun.com/tutorials/esp8266-thing-hookup-guide/using-the-arduino-addon

So first of all weather it is possible or not using HSPI to get response in slave mode from the ESP12E using any controller.

They are using #Include<ESP8266WiFi.h> file but i did not find this header file in arduino tool.

Requesting you to kindly provide this header file also

Thank you sir.

Regards

amarr