2014-07-22 1:53 AM
Hello,
I have a problem with the initialization of the SPI1 from my STM32F It doesn't work and I don't now what I doing wrong or what I forged. When I write something in the data Register ( SPI1->DR), nothing happens. The System Clock comes from per PLL from a HSE CLOCK. I hope someone can say me what I doing wrong. Sorry for my bad English.void init_spi_disp(void){
// ENABLEN DES GPIO FPR ALTERNATING FUNKTION
//RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;
#if 1
RCC->AHB1ENR |= RCC_AHB1ENR_CRCEN;
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; // ENABLE SPI 1FUNKTION CLOCK
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN | // PORT A ENABLE
RCC_AHB1ENR_GPIOBEN; // PORT B ENABLE
GPIOB->MODER |= GPIO_MODER_MODER4_0| // CS LCD as output
GPIO_MODER_MODER5_0; // CS SD as output
GPIOB->MODER &= ~( GPIO_MODER_MODER4_1 |
GPIO_MODER_MODER5_1 );
GPIOB->MODER |= GPIO_MODER_MODER10_0; // SET PB10 (DC) as Output
GPIOB->MODER &= ~GPIO_MODER_MODER10_1;
// SET OUTPUT SPEED AS FAST
GPIOA->OSPEEDR |= Bit10 | Bit11 |
Bit12 | Bit13 |
Bit14 | Bit15 ;
GPIOA->MODER |= GPIO_MODER_MODER5_1| // SET PA5 PA6 PA7
GPIO_MODER_MODER6_1 | // AS ALTERNATING FUNKTION
GPIO_MODER_MODER7_1;
GPIOA->MODER &= ~(GPIO_MODER_MODER5_0|
GPIO_MODER_MODER6_0|
GPIO_MODER_MODER7_0);
GPIOA->AFR[0] |= Bit20 | Bit22 | // SET ALTERNATING FUNKTION TO SPI1..4 (AF5)
Bit24 | Bit26 |
Bit28 | Bit30 ;
GPIOA->AFR[0] &= ~(Bit21 | Bit23|
Bit25 | Bit27 |
Bit29 | Bit31 );
// SET Default
SPI1->CR1 = 0;
SPI1->CRCPR = 7 ;
SPI1->CR1 &= ~( SPI_CR1_SPE); // DISABLE SPI
// Disable SPI for Register SET
SPI1->CR1 &= ~ (SPI_CR1_BIDIMODE) ; // SET SPI AS 2-line unidirectional mode
SPI1->CR1 &= ~ (SPI_CR1_CRCEN) ; // DISABLE CRC CALCULATION
SPI1->CR1 &= ~ ( SPI_CR1_DFF) ; // SET DATA FRAME TO 8 BIT DATA FRAME
SPI1->CR1 &= ~ ( SPI_CR1_RXONLY); // SET FULL DUPLEX
SPI1->CR1 |= SPI_CR1_SSM; // MUSS ICH DAS SETZEN ICH BIN DOCH MASTER ?????
#if 1 // DIV /4
SPI1->CR1 |= SPI_CR1_BR_0; // SPI DIVISION /4 for 21 MHZ Frequenc
SPI1->CR1 &= SPI_CR1_BR_1 |
SPI_CR1_BR_2 ;
#else // DIF 128
SPI1->CR1 |= SPI_CR1_BR_2|
SPI_CR1_BR_1;
SPI1->CR1 &= ~(SPI_CR1_BR_0);
#endif
/**FRAM FORMAT NOCH BETRACHTEN */
//SPI1->CR1 |= SPI_CR1_LSBFIRST ; // SET LSB TRAMSMISSION FIRST
SPI1->CR1 |= SPI_CR1_MSTR; // SPI is Master
SPI1->CR1 &= ~(SPI_CR1_CPOL|
SPI_CR1_CPHA);
SPI1->I2SCFGR &= ~(SPI_I2SCFGR_I2SMOD);
// INTERRUPTS NOT ENABLED
SPI1->CR1 |= (SPI_CR1_SPE); // ENABLE SPI1
#endif
}
2014-08-05 2:46 AM
I find it very disillusion that ST supports apparently only Problems with the CMSIS functions. That is for me in the future as an potential decider for bigger Hardware Projects very illuminating.
2014-08-05 4:16 AM
This is a User forum, the lack of response is illustrative only that those here have better things to do with our time than go over others register level code. If you want to code like this, then you really need to own responsibility for it.
2014-08-05 4:26 AM
I agree with Clive1.
Even when some good samaritan takes the time to read your unreadable code, he can not find your problem, simply because you did not say a word of what it is. I read the code, it looks good. So what ? you have a problem ? Start describing what make you thinking there is actually a problem, then someone might help you.