cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f401re nucleo: ADC question

life758
Associate II
Posted on December 02, 2015 at 11:44

Hello everybody,

I started to use the ADC and I'd like to use every features of this module.

While I read the reference manual and the datasheets i didn't found anything about using two input channels in differential mode. Did I miss something?

Regards
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on December 03, 2015 at 03:48

I'm not sure where you got the thought the F4 supported a differential mode. May be you're thinking about the F3

As I recall the F401 is a feature limited part, with only a single ADC, less memory, speed, timers, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
life758
Associate II
Posted on December 03, 2015 at 15:42

Thanks!