cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401 stop mode

matas
Associate II
Posted on September 03, 2015 at 17:18

Hey, I have encountered a interesting error. I have made a logger and to save power it goes to stop mode (~6-7ms), while the sensor is converting the results and to stand by mode (1-2s) till the next measurement. The datasheet says that while in stop mode the consumption should be ~40uA and in standby ~2-4uA. Now here is the question in standby mode the consumption is close to zero, while in stop mode it is ~20mA, so why? If the circuitry would be wrong the logger should always consume 20mA. The main code part looks like this:

  RTC_Config();

  PWR_EnterSTOPMode(PWR_LowPowerRegulator_ON, PWR_STOPEntry_WFI);

    

  

   RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);

  

  /* Allow access to Backup */

   

  PWR_BackupAccessCmd(ENABLE);

  

  RTC_WakeUpCmd(DISABLE);

        

  SYSCLKConfig_STOP();

  GPIO_ResetBits(GPIOB, GPIO_Pin_14);

 

  

  PWR_ClearFlag(PWR_FLAG_SB | PWR_FLAG_WU);

  RTC_WaitForSynchro();

  RTC_ClearFlag(RTC_FLAG_WUTF);

  jumperTime = 1020;

  

  RTC_SetWakeUpCounter(jumperTime); 

  RTC_WakeUpCmd(ENABLE);

      

  PWR_EnterSTANDBYMode();

on each wake up it initializeses the RTC settings, and after Stop mode just changes the sleep duration. Have any of you encountered this?
Foo Bar
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on September 05, 2015 at 14:26

How do you measure the current? Can't this be the consequence of the processor running at full throttle before and after the 5-6ms stop period? Don't you have the debugger connected?

JW