cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4 timer2 problem.

jbl_raw
Associate II
Posted on June 10, 2013 at 23:19

i used timer2 and it's clock source from  APB1   and Prescaler  value for  APB1 is 4

it's mean's APB1 work at 42mhz     ''168mhz/4 ''     becuase the maximum  frequency is 42mhz for APB1.

i searched in internet and some people write the timer2 clocked at 84mhz  not 42mhz and it's true.

but i cant find in this stm32f4 datasheet
1 REPLY 1
Posted on June 11, 2013 at 00:18

Yes, review the clock tree in the Reference Manual. For DIV2 on the APB it is DIV1 on the TIMCLK, for DIV4 on APB it is DIV2 on the TIMCLK

0690X00000605N7QAI.png

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..