STM32F4 PWM starting with different Polarity and shift time state
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-16 2:29 AM
Posted on May 16, 2015 at 11:29
Hi.
I work on STM32F4 MCU. For current project I work with 3 PWM are configured on TIM1 and Channels 1, 2, 3, GPIOs PE9, PE11, PE13.Every channel configured with 60 degrees shift. When I do ''Enable'' for all channelsTIM_CCxCmd
(TIM1, TIM_Channel_1, TIM_CCx_Enable);TIM_CCxCmd
(TIM1, TIM_Channel_2, TIM_CCx_Enable);TIM_CCxCmd
(TIM1, TIM_Channel_3, TIM_CCx_Enable); they are work with 60 degres shift as defined, but every start pulse can be started from different state - high or low in the 0-120 degrees time.How can I define PWM output that Channel1 will start every time with ''Enable'' channel and from low to high state (0 degrees delay), not shifted between 0-120 degrees.Thanks.This is my part code.voidGPIO_Configuration
(void){ GPIO_InitTypeDef GPIO_InitStructure; // GPIOE clock enableRCC_AHB1PeriphClockCmd
(RCC_AHB1Periph_GPIOE, ENABLE); //------------------------------------------------------------------------ // PWM GPIOs // Connect TIM1 pinsGPIO_PinAFConfig
(GPIOE, GPIO_PinSource9, GPIO_AF_TIM1); // PE9 TIM1_CH1GPIO_PinAFConfig
(GPIOE, GPIO_PinSource11, GPIO_AF_TIM1); // PE11 TIM1_CH2GPIO_PinAFConfig
(GPIOE, GPIO_PinSource13, GPIO_AF_TIM1); // PE13 TIM1_CH3 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_11 | GPIO_Pin_13; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;GPIO_Init
(GPIOE, &GPIO_InitStructure);}voidTIM1_Configuration
(uint32_t PWM_Frequency){ RCC_ClocksTypeDef RCC_ClocksStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; int Prescaler, Period; uint32_t TimerFrequency = 0; // enable peripheral clock for TIM1RCC_APB2PeriphClockCmd
(RCC_APB2Periph_TIM1, ENABLE); // Get clocksRCC_GetClocksFreq
(&RCC_ClocksStructure); // if(TIMx == TIM1) TimerFrequency = RCC_ClocksStructure.HCLK_Frequency; Prescaler = 1; Period = TimerFrequency / 2 / PWM_Frequency; // KHz // The toggle halves the frequency /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = Period - 1; TIM_TimeBaseStructure.TIM_Prescaler = Prescaler - 1; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseInit
(TIM1, &TIM_TimeBaseStructure); /* Output Compare Toggle Mode configuration: Channel 1, 2 and 3 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCPolarity_High; /* Default unused fields TIM1 more sensitive */ TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset; /* Don't want to set 0 or Period, but have 3 points at 120 degrees from each other */ TIM_OCInitStructure.TIM_Pulse = ((Period * 1) / 3) - 1;TIM_OC1Init
(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = ((Period * 2) / 3) - 1;TIM_OC2Init
(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = ((Period * 3) / 3) - 1;TIM_OC3Init
(TIM1, &TIM_OCInitStructure); /* Enable pins, TIM1 more sensitive */TIM_CtrlPWMOutputs
(TIM1, ENABLE); /* Configures the TIM1 Update Request Interrupt source (SETS the CR1->URS bit)*/TIM_UpdateRequestConfig
(TIM1,TIM_UpdateSource_Global); /* TIM1 enable counter */TIM_Cmd
(TIM1, ENABLE); // Disable ChannelsTIM_CCxCmd
(TIM1, TIM_Channel_1, TIM_CCx_Disable);TIM_CCxCmd
(TIM1, TIM_Channel_2, TIM_CCx_Disable);TIM_CCxCmd
(TIM1, TIM_Channel_3, TIM_CCx_Disable);}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0