STM32F4 problem with USART1 INTERRUPT
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-02-19 12:52 PM
Hi guys,
I have a problem with my new schede STM32F407VG. Until now I have been used the STM32F100B so now I'm adapting the code that I wrote. Part of my code is USART with interrupt, so I have wrote a code that read from USART1 (pin rx P10 and pin tx P9) and when the buffer is full the tx interrupt is ENABLE. I think that the configuration GPIO is wrong because I have modified only this part. If I send a string by Terminal I receive different data for example if I send sasdas I receive {\xfe}{\xfe}{\xfe}{\xf0}{\xfe}, I checked the baudrate on the Terminal and it is the same of the USART.I prefix that the code works on the STM32F100B, where the GPIO configuration is:GPIO_InitTypeDef GPIO_InitStructure;
/* Configure USART Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART Rx as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; // PA.10 USART1.RX GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure);How is the GPIO configuration for the STM32F4?? I'm very confused.The code write for the STM32F4 is this, where do I err???/* Includes ------------------------------------------------------------------*/
#include ''stm32f4xx.h''#include ''stm324xg_eval.h''char StringLoop[6];/**************************************************************************************/ void RCC_Configuration(void){ /* Enable GPIO clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Enable UART clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);} /**************************************************************************************/ void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; // Pin 10 Rx GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); // Pin 9 Tx GPIO_PinAFConfig( GPIOA, GPIO_PinSource9, GPIO_AF_USART1); /* Configure USART Tx as alternate function */ GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; //GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;//
Is it right??
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;////Is it right?? Should it be IN FLOATING????
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOA, &GPIO_InitStructure); } /**************************************************************************************/ void USART_Configuration(void){ USART_InitTypeDef USART_InitStructure; USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* USART configuration */ USART_Init(USART1, &USART_InitStructure); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); /* Enable the USART1 */ USART_Cmd(USART1, ENABLE); } /**************************************************************************************/ void NVIC_Configuration(void){ NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); NVIC_InitTypeDef NVIC_InitStructure; // Configure the NVIC Preemption Priority Bits NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); /* Enable the USART1 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);} /**************************************************************************************/int main(void){ RCC_Configuration(); GPIO_Configuration(); NVIC_Configuration(); USART_Configuration(); while(1){ } }/**************************************************************************************/void USART1_IRQHandler(void){ static int tx_index = 0; static int rx_index = 0; // Interrupt rx if (USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) { StringLoop[rx_index++] = USART_ReceiveData(USART1); if (rx_index >= (sizeof(StringLoop) - 1)) { rx_index = 0; USART_ITConfig(USART1, USART_IT_TXE, ENABLE); } } // Interrupt tx if (USART_GetITStatus(USART1, USART_IT_TXE) != RESET) { USART_SendData(USART1, StringLoop[tx_index++]); if (tx_index >= (sizeof(StringLoop) - 1)) {tx_index = 0; USART_ITConfig(USART1, USART_IT_TXE, DISABLE);} }} /**************************************************************************************/#ifdef USE_FULL_ASSERT/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { }}#endifTHANK!!- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-02-19 4:10 PM
USART1 PA9/PA10 is problematic on the STM32F4-Discovery due to a large bulk capacitor.
This should demonstrate the basic pin setup (GPIO and AF pin source mux)// STM32 USART IRQ TX/RX Loop (USART3 Tx PD.8, Rx PD.9) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
volatile char StringLoop[] = ''The quick brown fox jumps over the lazy dog
'';
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* GPIOD clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_USART3);
}
/**************************************************************************************/
void USART3_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART3, &USART_InitStructure);
USART_Cmd(USART3, ENABLE);
USART_ITConfig(USART3, USART_IT_RXNE | USART_IT_TXE, ENABLE);
}
/**************************************************************************************/
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Configure the NVIC Preemption Priority Bits */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);
/* Enable the USART3 Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/**************************************************************************************/
void USART3_IRQHandler(void)
{
static int tx_index = 0;
static int rx_index = 0;
if (USART_GetITStatus(USART3, USART_IT_TXE) != RESET) // Transmit the string in a loop
{
USART_SendData(USART3, StringLoop[tx_index++]);
if (tx_index >= (sizeof(StringLoop) - 1))
tx_index = 0;
}
if (USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) // Received characters modify string
{
StringLoop[rx_index++] = USART_ReceiveData(USART3);
if (rx_index >= (sizeof(StringLoop) - 1))
rx_index = 0;
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
NVIC_Configuration();
USART3_Configuration();
while(1); // Don't want to exit
}
/**************************************************************************************/
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
‎2013-02-20 2:03 AM
Thank you, I have just solved the problem. It isn't only due to ''
USART1 PA9/PA10 is problematic on the STM32F4-Discovery due to a large bulk capacitor
'' , in fact I tryed to use another USART but I had the same problem. It was due to HSE_VALUE that in my old schede STM32F100B is 8MHz but in the new STM32F4 is 25MHz , so I changed it in 8 MHz and now the USART1 PA6/PA7 finally works.THANK AGAIN- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-02-20 4:22 AM
The STM32F4-Discovery uses an 8 MHz crystal, HSE_VALUE always needs to reflect the hardware on your board. For other boards posting to the ''STM32 Discovery'' forum seems a bit odd, in the future posting to the ''STM32'' generic forum would be helpful, along with specific details about the board being used. Thanks.
Up vote any posts that you find helpful, it shows what's working..