cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4 mp45dt02 sampling above 16k not working

david239955
Associate II
Posted on December 22, 2013 at 14:55

Hello.

I'm using mp45dt02 mic on the discovery board and just forwarding data to cs43l22. For sampling freq 16k is working fine, but if I want higher Fs, it doesn't work anymore. I'm only hearing beeping/scratching from dac. Playing some 48k sound from flash works fine, so cs43l22 must be ok. I must be doing something wrong with the mic.

I can provide cs43l22 code and/or hex files if someone will be interested.

Here is the code for mp45dt02:

&sharpinclude <stdint.h>

&sharpinclude ''stm32f4xx.h''

&sharpinclude ''stm32f4xx_rcc.h''

&sharpinclude ''stm32f4xx_gpio.h''

&sharpinclude ''stm32f4xx_spi.h''

&sharpinclude ''pdm_filter.h''

&sharpinclude ''queve.h''

//sampling frequency

&sharpdefine FS 16000

//PDM decimation factor

&sharpdefine DECIMATION 64

//clock for mic

&sharpdefine I2S_CLK ((FS*DECIMATION)/(16*2))

//uint16_t array length for filter input buffer

&sharpdefine MIC_IN_BUF_SIZE ((((FS/1000)*DECIMATION)/8)/2)

//uint16_t array length for filter output buffer

&sharpdefine MIC_OUT_BUF_SIZE (FS/1000)

static PDMFilter_InitStruct pdm_filter;

static uint16_t mic_in_buf[MIC_IN_BUF_SIZE];

static uint16_t mic_out_buf[MIC_OUT_BUF_SIZE];

static uint32_t mic_buf_index;

void mp45dt02_init(){

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE);

pdm_filter.LP_HZ=8000;

pdm_filter.HP_HZ=10;

pdm_filter.Fs=FS;

pdm_filter.Out_MicChannels=1;

pdm_filter.In_MicChannels=1;

PDM_Filter_Init(&pdm_filter);

//MP45DT02 CLK-PB10

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);

GPIO_InitTypeDef gpio;

gpio.GPIO_Pin=GPIO_Pin_10;

gpio.GPIO_Mode=GPIO_Mode_AF;

gpio.GPIO_OType=GPIO_OType_PP;

gpio.GPIO_PuPd=GPIO_PuPd_NOPULL;

gpio.GPIO_Speed=GPIO_Speed_50MHz;

GPIO_Init(GPIOB, &gpio);

GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_SPI2);

//MP45DT02 DOUT-PC3

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

gpio.GPIO_Pin=GPIO_Pin_3;

gpio.GPIO_Mode=GPIO_Mode_AF;

gpio.GPIO_OType=GPIO_OType_PP;

gpio.GPIO_PuPd=GPIO_PuPd_NOPULL;

gpio.GPIO_Speed=GPIO_Speed_50MHz;

GPIO_Init(GPIOC, &gpio);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource3, GPIO_AF_SPI2);

NVIC_InitTypeDef nvic;

nvic.NVIC_IRQChannel = SPI2_IRQn;

nvic.NVIC_IRQChannelPreemptionPriority = 1;

nvic.NVIC_IRQChannelSubPriority = 0;

nvic.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&nvic);

//I2S2 config

RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

RCC_PLLI2SCmd(ENABLE);

while(!RCC_GetFlagStatus(RCC_FLAG_PLLI2SRDY));

I2S_InitTypeDef i2s;

i2s.I2S_AudioFreq=I2S_CLK;

i2s.I2S_Standard=I2S_Standard_LSB;

i2s.I2S_DataFormat=I2S_DataFormat_16b;

i2s.I2S_CPOL=I2S_CPOL_High;

i2s.I2S_Mode=I2S_Mode_MasterRx;

i2s.I2S_MCLKOutput=I2S_MCLKOutput_Disable;

I2S_Init(SPI2, &i2s);

I2S_Cmd(SPI2, ENABLE);

}

void mp45dt02_start(){

SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_RXNE, ENABLE);

}

void SPI2_IRQHandler(){

if(SPI_GetITStatus(SPI2, SPI_I2S_IT_RXNE)){

uint16_t sample=SPI_I2S_ReceiveData(SPI2);

mic_in_buf[mic_buf_index++]=HTONS(sample);

if(mic_buf_index == MIC_IN_BUF_SIZE){

mic_buf_index=0;

PDM_Filter_64_LSB((uint8_t *)mic_in_buf, mic_out_buf, 40, &pdm_filter);

uint32_t i;

for(i=0; i<MIC_OUT_BUF_SIZE; i++){

enqueve(mic_out_buf[i]);

}

}

}

}

Thanks.

#stm32f4discovery-mp45dt02
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
david239955
Associate II
Posted on December 31, 2013 at 15:27

Is my input and output buffer length correct?

I attached compiled program which in infinite loop firstly recording for 1 sec and then playing recorded sound. You can hear scratching. I also noticed that at record cycle dac sometimes outputs noise and sometimes nothing.

Compiler is gcc arm embedded 4.7 and I compiled with -Os

________________

Attachments :

mic_48k.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzni&d=%2Fa%2F0X0000000bPp%2FrSYLRaQGY.S63RWld382S_Z5wKJ7rWWqCyleV_vb97Y&asPdf=false
jainpl15
Associate
Posted on August 16, 2016 at 08:34

hey, i am working on the same project. Trying to capture audio and playing it back. I am facing a lot of issues trying to get it work. Can you please mail me the complete project with all the header and source files so that i can get a better understanding about it?

I would be highly obliged.

email-id : jainpl15.extc@coep.ac.in