cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 LTDC Color Depth

ktrofimo
Senior III
Posted on January 27, 2014 at 14:46

Hello!

I am using STM32F429 Discovery board with custom base board with VGA DAC. Everything is working, but it looks this chip has some limitations I could not find in the tech docs - 640x480@60Hz runs only in 16-bits modes (for example RGB565) and 800x600@60Hz runs in 8-bit modes (L8 or AL44)

Is there any documentation that describes maximum color depths for different resolutions?

Thank you!

Kirill
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0