cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 HSE clock frequency without HSE

Vasileios Amoiridis
Associate II
Posted on April 12, 2018 at 02:23

I am using an STM32F446ZE Nucleo Board which does NOT have an external HSE clock. From CubeMX I set the clock input from the HSE and after in the clock configuration I set the system clock to 180MHz.

https://i.stack.imgur.com/JyaEk.png

and in the clock configuration I set the PLL like this

https://i.stack.imgur.com/bxOm4.png

The code generated by CubeMX seems to be correct also.

https://i.stack.imgur.com/zyetq.png

My point is that even if I don't have an HSE in the board the uController works in 180MHz. How is this possible? What is the clock input after all?
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Make sure you are using the HSE in BYPASS mode in the clock settings.

You have to start the HSE, it will not start oscillating automatically. ie HSE_ON

If it doesn't oscillate most likely that your circuit characteristics are wrong.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..