STM32F4 (F4 discovery board) interrupt Issue
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-19 6:14 AM
Posted on May 19, 2014 at 15:14
Hi everybody,
I have an unstable behavior on an ADC interrupt.My user code is very simple, I initialize my different peripherals (timer, ADC, GPIO) then I just a have an infinite loop.My Callback for my ADC interrupt just get the ADC value. The ADC is configured to start conversion on a trigger from timer 2.I observe that the number of code lines in my program give two different result:- All is fine: I have a periodic IT on my ADC- Error: the Interrupt happens just one time and then never.The code lines I add to get the different behaviors are independent from the program, it can be variable initialization, variable indentation, ..As IDE i use IAR ewarm 6.30.
Any ideas whats wrong? I got no errors on the compiler, or debugger.Thanks for your help,
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-19 5:58 PM
Posted on May 20, 2014 at 02:58
We have had a lot of rain lately, so the cool morning fog seems to have clouded my crystal ball. Do you mind showing us the code for the error condition ?
Cheers, HalOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-20 12:37 AM
Posted on May 20, 2014 at 09:37
Hey Hal,
My code was generated with STM32Cube (I have attached the project file). In the options of the project, I delete optimizations of the code. Here is the function main with my user code: int main(void) { /* USER CODE BEGIN 1 */ uint8_t i = 0; /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ADC1_Init(); MX_I2S2_Init(); MX_TIM1_Init(); MX_TIM2_Init(); MX_USART3_UART_Init(); /* USER CODE BEGIN 2 */ HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET); HAL_ADC_Start_IT(&hadc1); HAL_TIM_OC_Start(&htim2, TIM_CHANNEL_1); /* USER CODE END 2 */ /* USER CODE BEGIN 3 */ /* Infinite loop */ while (1) { } /* USER CODE END 3 */ } Here is the callback of my ADC interrupt: /* USER CODE BEGIN 0 */ #define NB_MEAN_SAMPLE_PHOTODIODE 10000.0 uint8_t sEndRecord = 0; float sMeanPhotodiodePower = 0; uint8_t sDetectObject = 0; uint16_t sNbSamplePhotodiode = 0; float wADCValue = 0.0; void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) { if(sNbSamplePhotodiode < NB_MEAN_SAMPLE_PHOTODIODE) { sMeanPhotodiodePower = HAL_ADC_GetValue(hadc)/NB_MEAN_SAMPLE_PHOTODIODE + sMeanPhotodiodePower; sNbSamplePhotodiode ++; } else { if ((wADCValue=(float)HAL_ADC_GetValue(hadc))<(sMeanPhotodiodePower-30)) { sDetectObject ++; } else { sDetectObject = 0; } } } With this simple project, we can just enter once in the ADC interrupt. But If, for example, I comment if ((wADCValue=(float)HAL_ADC_GetValue(hadc))<(sMeanPhotodiodePower-30)) { sDetectObject ++; } else { sDetectObject = 0; } My ADC interrupt is periodically called. This workstooby commenting the configuration of an I/O For example this I/O: GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); Thanks for your interest, ________________ Attachments : MainProject.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0nZ&d=%2Fa%2F0X0000000bdm%2FfqwxhhCK5QAmQ.qMgTT00tFwVEoGEBsiuF6BLqPr7jQ&asPdf=falseOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-21 12:08 AM
Posted on May 21, 2014 at 09:08
This does not really explain how is the ADC triggered.
If you suspect this is a flaw in the Cube library, you should post in the dedicated sub-forum https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx JW