cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Discovery SPI Ethernet

vishaletm
Associate
Posted on February 14, 2013 at 14:54

Hello,

 

I need to connect an ENC28j60 module to STM32 Discovery. As there is some peripherals on board uses SPI for communication, i dont know which is the free to use SPI. I hope the SPIs used by peripherals is not available for our use!

 

 

Please provide a code snippet showing the respective SPI.

Regards

Vishal

 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on February 14, 2013 at 18:34

The board has manual and schematic, including a list of used pins, suggest you review those.

If there is a conflict you can always remove parts.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
Posted on February 15, 2013 at 08:55

Try searching the forum - various people have posted Excel sheets showing the pin usage of various discovery boards...

 

 

''Please provide a code snippet showing the respective SPI''

 

 

Have you looked at the SPI examples provided by ST (included in the firmware library)?
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
linas2
Associate II
Posted on February 15, 2013 at 09:48

Just download from www.st.com MicroXplorer, it has all Cortex M devices, with pinouts,  and functions, so you can design your board and don't have any conflicts

Andrew Neil
Super User
Posted on February 15, 2013 at 13:41

''download from www.st.com MicroXplorer ... you can design your board and don't have any conflicts''

But he specifically stated that he's using a Discovery Board! So that's no help - is it?!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.