Question
Stm32f4 Discovery-Change the duty cycle with user button-Help
Posted on July 09, 2013 at 10:52
Hello everyone,I am the new user and I need your help about an example Stm32f4- Discovery.I use TIM10 register for to get pwm.And I want to be increase duty ratio with user button.I try to change TIM10->CCR1 but its not working.What should I do for this problem??;Here is my code:
/* TIM10_PWM * main.c * * Created on: 12 Agu 2012 * Author: m2k */&sharpinclude ''stm32f4xx.h''GPIO_InitTypeDef GPIO_InitStructure;TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;TIM_OCInitTypeDef TIM_OCInitStructure;uint16_t PrescalerValue = 0; void GPIO_Conf(void) { /* GPIOB ve TIM10 CLK Kaynagi etkinlestiriliyor */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB,ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM10,ENABLE); /* PB8 Ek �zellikler i�in ayarlaniyor */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &GPIO_InitStructure); /*Pin Y�nlendirme Islemi*/ GPIO_PinAFConfig(GPIOB,GPIO_PinSource8,GPIO_AF_TIM10);} void TIM_Conf(void) {int val=0; PrescalerValue = 140; /* TIM10 Ayarlari Yapiliyor */ TIM_TimeBaseStructure.TIM_ClockDivision = 0; /* TIM10 I�in CounterMode_UP Gereksizdir. Fakat Kodu degistirip * diger sayicilar i�in kullanma ihtimaline karsi silmiyorum */ TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 10; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseInit(TIM10, &TIM_TimeBaseStructure); /* PWM Ayarlari yapiliyor. 32KHz @ %50 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM10->CCR1=val; TIM_OC1Init(TIM10, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM10, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM10, ENABLE); }int main(void) { int val=0; TIM10->CCR1=val; if(GPIO_ReadInputDataBit(GPIOA,GPIO_Pin_0)) { val++; } GPIO_Conf(); TIM_Conf(); /* TIM10 Baslatiliyor */ TIM_Cmd(TIM10, ENABLE); while(1){ } } #stm32f4-discovery-timer10-duty