cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 DIS CAM on the STM32F4 Discovery Board

fabian2
Associate
Posted on July 29, 2015 at 10:56

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
1 REPLY 1
fabian2
Associate
Posted on August 05, 2015 at 14:22

Solved the problem. It was an issue with the SystemCoreClock beeing too slow. It was at 1MHz, which wasn't enough to provide enough Data in a short time. I upped the frequency to 144MHz, as done in the example code, and now it works.