cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 connect to Network printer

pic_micro
Associate II
Posted on March 29, 2015 at 07:55

Dear All,

When I enter the IP address of my network printer on web browser, it shows page which contains print counter and more  which I taken prints from the printer. So my project is connect the STM32F4 MCU to network printer then show the copy counter on the LCD

Please advise to success this project 

Please advise step to I should follow

Thanks in advance 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
tm3341
Associate II
Posted on March 29, 2015 at 13:01

You can configure your STM device with ethernet.

Then, you can periodically make connections to your known IP for your printer.

You can use TCP requests as a CLIENT to your printer which is SERVER.

Data he returns you back (print counter and so on) you parse easily and display on LCD.

This library should help you a lot for ethernet using TCP client: 

http://stm32f4-discovery.com/2015/02/library-52-ethernet-peripheral-on-stm32f4xx/

pic_micro
Associate II
Posted on March 29, 2015 at 16:03

Dear majerle Thanks for the reply

That mean can we access the printer data without browser 

francescatodiego
Associate II
Posted on March 29, 2015 at 17:58

You can check the page html source code when you access printer with browser.

The page contain a request for printer data (counter...).

Form the STM device you must send this http request (post or get to the printer) and decode the printer reply

With firefox browser the traffic request/reply can be easily view with firebug addon

But also wireshark can be used for traffic analysis