Question
STM32F373 SDADC HAL after Calibration, do I need to manual put an offset error value to final calculate with sdadc output value?
Hi
As a title, after I call
HAL_SDADC_CalibrationStartand
HAL_SDADC_PollForCalibEventfollow Refference Manual page 240, calibration progress will store an offset error value in OFFSETx[11:0] fields. So do I need to read this value and put in the calculation (minus or plus) after read SDADC output value? Or it is automatically calculated and I just use the SDADC output value?
For Gain Calibration, I have to manually read data and calculate the gain value, and put into final calculation, right?
Thanks so much