2015-08-31 8:45 AM
Hi,
I use TIM1 PWM in asymmetric mode. I need to switch between 2 software modes : Mode A - CH1/1N asym mode 2, CH3/3N asym mode 2 Mode B - CH1 asym mode 1, CH3 asym mode 2, CH1N/3N off I use HAL for initialization but I need the transition between these 2 modes to be as quick as possible (and HAL is troubling me a bit) : Transition to mode A :// disable PWMs
htim1.Instance->CCER &= ~( TIM_CCER_CC1E
| TIM_CCER_CC1NE
| TIM_CCER_CC3E
| TIM_CCER_CC3NE );
htim1.Instance->BDTR&= ~TIM_BDTR_MOE;
htim1.Instance->CR1 &= ~TIM_CR1_CEN;
// configure
htim1.Instance->BDTR |= TIM_BDTR_DTG & TIM1_FREQ / DEAD_TIME_INVERSE;
htim1.Instance->CCMR1 |= TIM_CCMR1_OC1M & TIM_OCMODE_ASSYMETRIC_PWM2
| TIM_CCMR1_OC2M & TIM_OCMODE_ASSYMETRIC_PWM2 << 8;
htim1.Instance->CCR1= 0;
htim1.Instance->CCR2= htim1.Instance->ARR;
htim1.Instance->CCR3= x;
htim1.Instance->CCR4= y;
// enable PWMs
htim1.Instance->CCER |= TIM_CCER_CC1E
| TIM_CCER_CC1NE
| TIM_CCER_CC3E
| TIM_CCER_CC3NE;
htim1.Instance->BDTR|= TIM_BDTR_MOE;
htim1.Instance->CR1 |= TIM_CR1_CEN;
Transition to mode B :
// disable PWMs
htim1.Instance->CCER &= ~( TIM_CCER_CC1E
| TIM_CCER_CC1NE
| TIM_CCER_CC3E
| TIM_CCER_CC3NE );
htim1.Instance->BDTR&= ~TIM_BDTR_MOE;
htim1.Instance->CR1 &= ~TIM_CR1_CEN;
// configure
htim1.Instance->BDTR &= ~TIM_BDTR_DTG;
// remove deadtime
htim1.Instance->CCMR1 |= TIM_CCMR1_OC1M & TIM_OCMODE_ASSYMETRIC_PWM1
| TIM_CCMR1_OC2M & TIM_OCMODE_ASSYMETRIC_PWM1 << 8;
htim1.Instance->CCR1= 300;
htim1.Instance->CCR2= 0;
htim1.Instance->CCR3= htim1.Instance->ARR;
htim1.Instance->CCR4= htim1.Instance->ARR - htim1.Instance->CCR1;
// enable PWMs
htim1.Instance->CCER |= TIM_CCER_CC1E
| TIM_CCER_CC3E;
htim1.Instance->BDTR|= TIM_BDTR_MOE;
htim1.Instance->CR1 |= TIM_CR1_CEN;
The problem is : mode A looks ok, but when in mode B channel 1 stays in asymmetric PWM mode 2.
I tried a lot of things, including trying similar code with HAL_PWM_Start/Stop and other things. Sometimes channel 1 switches to asym mode 1 as needed, but it looks like chance.
One more thing : I initialize all channels in PWM asym mode 2 with HAL. But when I initialize CH1/2 in mode 1 and CH3/4 in mode 2, it works better, I don't know why.
Thanks in advance.
2015-08-31 1:19 PM
htim1.Instance->CCMR1 |= TIM_CCMR1_OC1M & TIM_OCMODE_ASSYMETRIC_PWM1
| TIM_CCMR1_OC2M & TIM_OCMODE_ASSYMETRIC_PWM1 << 8;
The
TIM_CCMR1_OC1M
bits are already all set from being set for PWM2 in previous step. You perhaps wanted to use = rather than |=.
Also, aren't the channel3 bits in CCMR2?
(I personally woldn't mix in the constants defined in CUBE (e.g.
TIM_OCMODE_ASSYMETRIC_PWM1
) and would stick to the constants defined in the basic CMSIS device header stm32f3xx.h, but that's me.)
JW
2015-08-31 11:47 PM
Indeed, the problem was the operator...
Thank you very much ! I feel a bit stupid x)